Trouble with KinetisFlashTool test with FRDM-K64F

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Trouble with KinetisFlashTool test with FRDM-K64F

2,064件の閲覧回数
chadwilliams
Contributor III

I have been attempting to use the KinetisFlashTool.exe tool  from the Bootloader version 2.0.0

Located at:

\NXP_Kinetis_Bootloader_2_0_0\bin\Tools\KinetisFlashTool\win

When I compile the following demo :

\NXP_Kinetis_Bootloader_2_0_0\apps\led_demo\MK64F12\kds\led_demo_freedom_a000

and create a .bin file, and try to update the board with it,

In the Log window of the dialog I see this:

Connected to device successfully!

Collecting device information......

Device information is updated!

Start update progress......

Updating image......

Error: Update image failed(kStatusMemoryRangeInvalid).

Update process is stopped by error.

I have tried the various file formats such as srec and hex and also set the target address to 0xa000

And also tried the same demo that's targetd to 0x0000

But in all cases, I receive the above error.  I am using the USB HID interface.

Has anyone successfully tested the KinetisFlashTool out of the box and can advise if it works?

2 返答(返信)

1,707件の閲覧回数
bileldrira
Contributor II

Hi, Chad. Have you found a solution ? I have the same issue with k64.

0 件の賞賛
返信

1,707件の閲覧回数
miduo
NXP Employee
NXP Employee

Hi,

Have you tried the released binary: NXP_Kinetis_Bootloader_2_0_0\targets\MK64F12\iar\binaries\freedom_bootloader.bin?  Does this file work?

0 件の賞賛
返信