Trouble resetting CnV register of FTM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Trouble resetting CnV register of FTM

2,218件の閲覧回数
konrada_anton
Contributor III

Hello all,

 

I'm writing an unloadable driver for the PWM functionality of the FTM of my K60 (using the TWRK60N512 and CodeWarrior). When unloading the driver, I want it to leave the FTM and all channels in a clean state so that the next user of the PWM facility cannot ever get a first cycle with yesterday's stale duty cycle. However, I can't manage to make the value of CnV stick.

 

Code snippet (uses MQX delay function, otherwise bare metal):

  uint_32 dummy;  FTM_MemMapPtr pRegs = FTM0_BASE_PTR;  // 1. switch on the clocks  // a. for the port module  SIM_SCGC5 |= SIM_SCGC5_PORTC_MASK;  // b. for the FTM  SIM_SCGC6 |= SIM_SCGC6_FTM0_MASK;  // configure port multiplexer   PORTC_PCR1 = PORT_PCR_MUX(4);  PORTC_PCR2 = PORT_PCR_MUX(4);  // a. make writable (must read bit WPEN of FTMx_FMS,   // then write a 1 to WPDIS of FTMx_MODE)  dummy = pRegs->FMS;  pRegs->MODE |= FTM_MODE_WPDIS_MASK;  // b. clear FTMEN flag, requires WPDIS to be set.  pRegs->MODE &= ~FTM_MODE_FTMEN_MASK;    // c. disable quadrature encoder  pRegs->QDCTRL &= ~FTM_QDCTRL_QUADEN_MASK;  // d. reset counter  pRegs->CNT = 0;    pRegs->MOD = 6000;   pRegs->CNTIN = 0; // counter starts at 0, nothing fancy    FTM0_C1V = 1000;  // set Prescaler and use so-called system clock.  FTM0_SC = (3 & FTM_SC_PS_MASK)     | (0x1 << FTM_SC_CLKS_SHIFT) // FTM system clock, i.e. Kinetis bus-clock    ;      FTM0_C1SC =         (0 << FTM_CnSC_DMA_SHIFT)  | (0 << FTM_CnSC_ELSA_SHIFT )  | (1 << FTM_CnSC_ELSB_SHIFT )  | (0 << FTM_CnSC_MSA_SHIFT )  | (1 << FTM_CnSC_MSB_SHIFT )  | (0 << FTM_CnSC_CHIE_SHIFT );     FTM0_C1V = 4000;   _time_delay(5000);  // turn your head towards the oscilloscope    // shut down the counter  FTM0_SC = 0;   // shut down the channel  FTM0_C1SC = 0;  FTM0_C1V = 0;    _time_delay(10); // let it settle  _time_delay(1000);

I expect the debugger to read FTM0_C1V as 0 after the line "let it settle". At least that's what I've concluded from The Book, chapter 39.4.10.3, "CnV Register Update", verse "If CLKS[1:0]=0:0 then CnV register is updated when CnV register is written". However, I still read the old value.

In order to minimize debugger impact on FTM, I've only set breakpoints before the 5000ms delay and after the "let it settle".

Am I doing it wrong, is the FTM wrong, is the debugger wrong, or should I just not worry about stale PWM cycles?

Thanks in advance, KA.

0 件の賞賛
返信
3 返答(返信)

1,616件の閲覧回数
konrada_anton
Contributor III

Thanks to the effects of having posted a public question, I've found a sequence which works:

  1. Stop the clock (CLKS=0)
  2. Write the desired 0 to CnV while the channel is still enabled.
  3. Disable the channel in CnSC

 

0 件の賞賛
返信

1,616件の閲覧回数
gtoph
Contributor II

I had a similar problem.  There are actually a few ways you could do it, depending on your needs.  Look for "Register Update"  under the FTM section in the manual for your particular chip and you'll see the options you have.

0 件の賞賛
返信

1,616件の閲覧回数
konrada_anton
Contributor III

I also tried enabling the advanced FTM registers in order to perform a software trigger, with no better results. Perhaps if I had combined that attempt with the reversed order of the access to CnSC and CnV, it would have worked. Whatever -- I only need very basic EPWM.

0 件の賞賛
返信