Tring to flash K10 from binary or read flash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Tring to flash K10 from binary or read flash

1,495 Views
Fred_Eric
Contributor I

Hello,

I am not familiar with the K10 and I am trying to figure out how to flash it from a binary file that I have (this binary is a file that is read by a touchscreen controller connected to the main board having the K10).

Another option could be to read from another board as I have few working boards. 

I have tried few things (converted the binary then flash it) but never got any success. I have done the same kind of thing with boards with PIC easily but this one is new to me.

I also tried to connect the controller to the board with a brand new K10 but the touch screen controller is not seeing the board (probably because there's now firmware and boot loader).


Thanks!

Fred

 

Labels (1)
0 Kudos
Reply
1 Reply

1,463 Views
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hello Fred,

 

Hope you are doing well. If you have your code project, you can use an external Debugger/Programmer.

 

Just, be sure that the Debug interface is correct. Please refer to section 2.1.5.3 of KQRUG, Kinetis K Quick Reference User Guide.

 

Regards,

Ricardo

0 Kudos
Reply