Trigger ADC with PDB from eFlexPWM - KV44F256x

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Trigger ADC with PDB from eFlexPWM - KV44F256x

ソリューションへジャンプ
1,847件の閲覧回数
katha
Contributor II

Hello,

is there an example code of how to trigger ADC via PDB from eFlexPWM with a KV44F256x?

Is there a possibility to get Peripherals tool for KV44F256x?

(code example for eFlexPWM for KV44F256x like in AN4410)

Regards

Katharina

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,748件の閲覧回数
FelipeGarcia
NXP Employee
NXP Employee

Hi Katharina,

 

You can take as reference the following application note. I believe it may be helpful for you.

https://www.nxp.com/docs/en/application-note/AN5237.pdf 


Have a great day,
Felipe

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,749件の閲覧回数
FelipeGarcia
NXP Employee
NXP Employee

Hi Katharina,

 

You can take as reference the following application note. I believe it may be helpful for you.

https://www.nxp.com/docs/en/application-note/AN5237.pdf 


Have a great day,
Felipe

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信