Transmiting a buffer on UART with DMA

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Transmiting a buffer on UART with DMA

ソリューションへジャンプ
6,760件の閲覧回数
john71
Senior Contributor I

Right now I transmit a buffer by blocking method

 

send_log_data_uart0(log_buffer_data, page_chunk);

 

Now I have to send it using DMA.

 

void DMA_Init(void)
{
	//enable clock for DMAMUX and DMA
	SIM_SCGC6 |= SIM_SCGC6_DMAMUX0_MASK;
	SIM_SCGC7 |= SIM_SCGC7_DMA_MASK;

	//enable channel 0 and set the source - 3 = UART0 Transmit ($3.3.9.1 Table 3-26)
	DMAMUX0_CHCFG0 |= DMAMUX_CHCFG_ENBL_MASK | DMAMUX_CHCFG_SOURCE(3);

	//set memory address for source and destination
	DMA_TCD0_SADDR = (uint32_t)&log_buffer_data;  //global scope buffer
	DMA_TCD0_DADDR = (uint32_t)&UART0_D;

    //set an offset
	DMA_TCD0_SOFF = 0;  //???
	DMA_TCD0_DOFF = 0;  //???

	//set data transfer size - byte
	DMA_TCD0_ATTR = DMA_ATTR_SSIZE(0) | DMA_ATTR_DSIZE(0);  //???

	//number of bytes to be transfered in each service request
	DMA_TCD0_NBYTES_MLNO = glob_data_chank;  //???

	//current major iteration count (a single iteration)
	DMA_TCD0_CITER_ELINKNO = DMA_CITER_ELINKNO_CITER(1);  //???
	DMA_TCD0_BITER_ELINKNO = DMA_BITER_ELINKNO_BITER(1);  //???

	DMA_TCD0_SLAST = 0;   //???
	DMA_TCD0_DLASTSGA = 0; //???

	//setup control and status register
	//DMA_TCD0_CSR = 0;

	//interrupt when tx/rx buffer is full. stop DMA on single transfer.
	DMA_TCD0_CSR = DMA_CSR_INTMAJOR_MASK | DMA_CSR_DREQ_MASK;
	//enable request signal for channel 0
	DMA_ERQ = DMA_ERQ_ERQ0_MASK;
}

 

So I have some questions.

1. Those registers with a question sign (//???) - is it configured OK?

2. buffer size can be changed (glob_data_chank). Should I update the DMA_TCD0_NBYTES_MLNO on every service request?

3. How do I set a DMA interrupt? Do I need the interrupt? I can poll the done flag

 

while (DMA_TCD0_CSR & DMA_CSR_DONE_MASK)

 

4. Do I need any additional setup on UART side? Do I need these lines?

 

UART0_C2 |= UART_C2_TIE_MASK;
UART0_C5 |= UART_C5_TDMAS_MASK;

 

5. How do I start a new transaction? Like this?

 

DMA_TCD0_CSR |= DMA_CSR_START_MASK;

 

0 件の賞賛
返信
1 解決策
6,693件の閲覧回数
PabloAvalos
NXP TechSupport
NXP TechSupport

Hello, @john71 

 

First of all, I am very thankful for your patience.

 

Then, I would like to know, which mcu are you using for?

Sharing with you a couple of threads of our community, where you can find accurate information on how DMA works. I would like to help you by telling you if the configuration of your registers with a question sign (//???) are configured ok, but it depends on your application needs.

 

Hoping this links might be helpful:

https://community.nxp.com/t5/Kinetis-Microcontrollers/UART-DMA-Configuration/m-p/1166667

https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K60-K70-configuration-of-DMA-with-I2S-...

 

At last but not least, regarding your other questions, the register DMA_TCD0_NBYTES_MLNO defines the number of bytes to transfer per request, so if you are going to change the data size to transfer in every request, you should update this register. For DMA interruption, you can refer to this link Interrupt on DMA Completion where is being used a Kinetis  K27 Series. Lastly, I will suggest you to check our SDK Examples, by searching and downloading your mcu sdk here: SDK Builder, where you can get functional examples on eDMA and DMA transfers in our MCUXpresso IDE.

Please let me know if you have more questions.

 

Best Regards.

Pablo Avalos.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
6,693件の閲覧回数
PabloAvalos
NXP TechSupport
NXP TechSupport

Hello, @john71 

 

First of all, I am very thankful for your patience.

 

Then, I would like to know, which mcu are you using for?

Sharing with you a couple of threads of our community, where you can find accurate information on how DMA works. I would like to help you by telling you if the configuration of your registers with a question sign (//???) are configured ok, but it depends on your application needs.

 

Hoping this links might be helpful:

https://community.nxp.com/t5/Kinetis-Microcontrollers/UART-DMA-Configuration/m-p/1166667

https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K60-K70-configuration-of-DMA-with-I2S-...

 

At last but not least, regarding your other questions, the register DMA_TCD0_NBYTES_MLNO defines the number of bytes to transfer per request, so if you are going to change the data size to transfer in every request, you should update this register. For DMA interruption, you can refer to this link Interrupt on DMA Completion where is being used a Kinetis  K27 Series. Lastly, I will suggest you to check our SDK Examples, by searching and downloading your mcu sdk here: SDK Builder, where you can get functional examples on eDMA and DMA transfers in our MCUXpresso IDE.

Please let me know if you have more questions.

 

Best Regards.

Pablo Avalos.

0 件の賞賛
返信
6,683件の閲覧回数
john71
Senior Contributor I

Thank you

0 件の賞賛
返信
6,727件の閲覧回数
john71
Senior Contributor I

Nobody knows how DMA works?

 

0 件の賞賛
返信