Touchscreen and ADC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,085件の閲覧回数
joelesco
Contributor III

Hi !

I use a K70 and I would like to plug a display wich comport a touchscreen. Do i need to use a controller between the touchscreen and the K70 or i can directly plug the touchscreen to ADC pins ?

Thanks a lot !

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
1,874件の閲覧回数
LuisCasado
NXP Employee
NXP Employee

Hello Jay,

No, you don't need a dedicated controller, you can use ADC and GPIO. CRTOUCH used in the TWR-LCD-RGB have extra functions like gesture recognitions.

Best Regards,

Luis

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,875件の閲覧回数
LuisCasado
NXP Employee
NXP Employee

Hello Jay,

No, you don't need a dedicated controller, you can use ADC and GPIO. CRTOUCH used in the TWR-LCD-RGB have extra functions like gesture recognitions.

Best Regards,

Luis

0 件の賞賛
返信
1,874件の閲覧回数
mjbcswitzerland
Specialist V

Hi

There is a guide to using resistive touch screens with ADC/GPIO here: http://www.utasker.com/docs/uTasker/uTaskerTouch.PDF

Regards

Mark

0 件の賞賛
返信