Toggle LED using a push button and FRDM-K64F?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Toggle LED using a push button and FRDM-K64F?

5,947 次查看
dayakannan
Contributor I

Hi.

I decided to venture into embedded systems very recently and enthusiastically got a new K64F board. I was able to manage a Blinky using youtube tutorials -  but I don't understand what's happening behind the scenes, so to speak (please excuse my non-technical usage of words, I'm very new).

I now want to write a program to toggle an LED using a push button. I have been searching all over the internet for tutorials that can help me figure out what to do and how to do it but haven't found anything yet.

Could anybody please help me with this? I would like to know where to find more information about the board I have and where to go online to start experimenting with this.

Thank you :smileyhappy:

- Daya

标记 (3)
0 项奖励
回复
2 回复数

2,936 次查看
BlackNight
NXP Employee
NXP Employee

I have a tutorial for the FRDM-KL25Z here:

http://mcuoneclipse.com/2012/11/12/tutorial-bits-and-pins-with-kinetis/

As that board shares the button with the reset function of the board, simply ignore the part about the reset line :-)

0 项奖励
回复

2,936 次查看
mjbcswitzerland
Specialist V

Daya

See http://www.utasker.com/kinetis/FRDM-K64F.html

You can toggle using push buttons on the board or buttons on a web page using a web browser.

Tutorial at http://www.utasker.com/docs/KINETIS/uTaskerV1.4_Kinetis.pdf

Simulate your board and the K64 in real-time with VisualStudio to learn all internal workings (including peripherals, interrupts, DMA and memory operations).

Regards

Mark

Kinetis: µTasker Kinetis support

K64: µTasker Kinetis FRDM-K64F support / µTasker Kinetis TWR-K64F120M support

For the complete "out-of-the-box" Kinetis experience and faster time to market

0 项奖励
回复