There is a I2S Project Example for K22F and SGTL5000?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

There is a I2S Project Example for K22F and SGTL5000?

1,373件の閲覧回数
matheus_pinto
Contributor II

Hello,

There is a I2S Project Example for K22F communicating with SGTL5000, especially that use KSDK 2.0 or Processor Expert?

I am having issues in implementation and I dont know if the problem is my software or the hardware (the components that I soldered on the FRDM-K22F board).

Thanks,

Matheus

タグ(3)
0 件の賞賛
返信
1 返信

1,231件の閲覧回数
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Matheus Pinto 

You could base your application code in the SAI example of the TWR-K22F120M that comes with the SDK 2.x package, it uses the SGTL5000.

Hope this could help.
Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信