The question about km34z256vll7 AFE module

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

The question about km34z256vll7 AFE module

1,639件の閲覧回数
小勇邹
Contributor II

Hi,
I am using km34z256vll7 in my project. In the ΣΔ ADC + PGA specifications, the
VCM range is 0~0.8V and VINdiff range is
±500mV(gain=1).

And I want to know if the input voltage over the range but under VDD,
will the  AFE module
  be damaged?

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,476件の閲覧回数
michael_galda
NXP Employee
NXP Employee

Hi Robin,

No the AFE itself won't be damaged, but the ADC result will be saturated, so you will be unable to measure the voltages above the specified range.

You are right that it must be below VDD.

Thanks,

Michael

0 件の賞賛
返信

1,476件の閲覧回数
jeff-jianfeng_l
Contributor II

Hi Michael,

Can you tell me the maximum and minimum input range of the AFE pins,if my input voltage is below zero, such as -2V,will the AFE damaged?

Thanks

Jeff

0 件の賞賛
返信