The question about km34z256vll7 AFE module

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The question about km34z256vll7 AFE module

1,694 Views
小勇邹
Contributor II

Hi,
I am using km34z256vll7 in my project. In the ΣΔ ADC + PGA specifications, the
VCM range is 0~0.8V and VINdiff range is
±500mV(gain=1).

And I want to know if the input voltage over the range but under VDD,
will the  AFE module
  be damaged?

Labels (1)
0 Kudos
Reply
2 Replies

1,531 Views
michael_galda
NXP Employee
NXP Employee

Hi Robin,

No the AFE itself won't be damaged, but the ADC result will be saturated, so you will be unable to measure the voltages above the specified range.

You are right that it must be below VDD.

Thanks,

Michael

0 Kudos
Reply

1,531 Views
jeff-jianfeng_l
Contributor II

Hi Michael,

Can you tell me the maximum and minimum input range of the AFE pins,if my input voltage is below zero, such as -2V,will the AFE damaged?

Thanks

Jeff

0 Kudos
Reply