The question about K64

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

The question about K64

1,608件の閲覧回数
小勇邹
Contributor II

My device is MK64FN1M0VMD12.The hardware is TWR-K64F120M. My compiler is IAR 7.2.

I have write a bootloader.

There are two parts for my program.


 

Boot loader 1


 

 

INTERRUPT VECTOR TABLE


 

 

1KB($00000000-$000003FF)


 

 

NONVOLATILE REGISTERS(FLASH CONFIGURATION)


 

 

16 bytes ($00000400-$0000040F)


 

 

BOOT LOADER 1


 

 

3056 bytes($00000410-$00000FFF)


 

 

Boot loader 2


 

 

RELOCATED INTERRUPT VECTOR TABLE


 

 

1KB($00001000-$000013FF)


 

 

BOOT LOADER 2


 

 

31KB($00001400-$00008FFF)


 

I write the program in the Boot loader 1 to jump to Boot loader 2.

  #define RELOCATED_VECTORS 0x1000

 

SCB_VTOR =
RELOCATED_VECTORS;

JumpToUserApplication(*((unsigned
long*)RELOCATED_VECTORS), *((unsigned long*)(RELOCATED_VECTORS+4)));

void JumpToUserApplication(LWord userSP, LWord userStartup)

{

// set up stack
pointer

  __asm("msr msp, r0");

  __asm("msr psp, r0");

  // Jump to PC (r1)

  __asm("mov pc, r1");

}             

Before I adding the source code(as follow shown). The Boot loader 1 jumps to Boot loader 2 normally.

__root const unsigned char FlashCheck1_user @ 0x2fff ;

__root const unsigned char FlashCheck2_user @ 0x4fff;

__root const unsigned char FlashCheck3_user @ 0x6fff;

__root const unsigned char FlashCheck4_user @ 0x8fff;

After I adding the source code(as follow above). The Boot loader 1 can not  jumps to Bootloader 2 normally.

Sometimes the program runs normally.But sometimes the program cannot run normally.It stops in
the source code(as shown below) of Boot loader 2.

while((MCG->S & MCG_S_LOCK0_MASK) == 0x00U) { /* Wait
until PLL is locked*/  }

Can anyone tell me the reason? Thank you very much.

0 件の賞賛
返信
2 返答(返信)

1,407件の閲覧回数
mjbcswitzerland
Specialist V

Hi

If your boot loader (1) configures the PLL you may need to be sure that the code in the application (boot loader 2) used to configure it (again) doesn't 'assume' that the PLL control (clock state) is in its reset state. It needs to be able to handle starting in one of the other clock states.

Therefore I would review the PLL configuration code in the application to see whether it can reliably handle thiks.

Regards

Mark

P.S. If the boot loader (1) is configuring the PLL to the frequency needed by the apllication the application doesn't need any PLL configuration code of its own.

0 件の賞賛
返信

1,407件の閲覧回数
小勇邹
Contributor II

Hello Mark,

The source code of the PLL configuration for  both bootloader (1) and Bootloader 2  is the same. The source code is in the attachment.

0 件の賞賛
返信