The frequency of MK60 twice low then expected

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The frequency of MK60 twice low then expected

Jump to solution
1,589 Views
nataliyadoni
Contributor I

I'm creating the project with MK60FN1M0VLQ15. I use external clock 25MHz.

When I move from PEI mode to PEE mode 150 MHz, I have got MCGCLKOUT 75 MHz (on TRACE_CLKOUT 18,8 MHz, on FB_CLK 25MHz).

But I've expected 150 MHz.

MCGCLKOUT=25 MHz*18/3

VDIV0=0x02 (18), PRDIV=0x02 (3).

But I have got 150 MHz only when VDIV0=0x14 (36).

What is it? An error in datasheat or my error?

Please, help me to find a mistake!

This my code:

  MCG_C2 = 0;
  MCG_C1 = MCG_C1_CLKS(2) | MCG_C1_FRDIV(3);
  /* if we aren't using an osc input we don't need to wait for the osc to init */
   MCG_C5 = 0;
   MCG_C5 = MCG_C5_PRDIV(2)|MCG_C5_PLLCLKEN_MASK;
  while (MCG_S & MCG_S_IREFST_MASK){}; // wait for Reference clock Status bit to clear

  while (((MCG_S & MCG_S_CLKST_MASK) >> MCG_S_CLKST_SHIFT) != 0x2){}; // Wait for clock status bits to show clock source is ext ref clk

// Now in FBE

  // Ensure MCG_C6 is at the reset default of 0. LOLIE disabled, PLL disabled, clk monitor disabled, PLL VCO divider is clear
  MCG_C6 = 0x0;

// Set system options dividers 150 МГц
      //MCG=PLL, core = MCG, bus = MCG/2, FlexBus = MCG/3, Flash clock= MCG/6
       set_sys_dividers(0,1,2,5);
      // Set the VCO divider and enable the PLL , LOLIE=0, PLLS=1, CME=0, VDIV=18   
      MCG_C6 = MCG_C6_PLLS_MASK | MCG_C6_VDIV(0x2); //M = 18  R =3 mcgoutclk=fext*m/r
      pll_freq = 150;
  while (!(MCG_S & MCG_S_PLLST_MASK)){}; // wait for PLL status bit to set

  while (!(MCG_S & MCG_S_LOCK_MASK)){}; // Wait for LOCK bit to set
// Now running PBE Mode
// Transition into PEE by setting CLKS to 0
// CLKS=0, FRDIV=3, IREFS=0, IRCLKEN=0, IREFSTEN=0
  MCG_C1 &= ~MCG_C1_CLKS_MASK;

// Wait for clock status bits to update
  while (((MCG_S & MCG_S_CLKST_MASK) >> MCG_S_CLKST_SHIFT) != 0x3){};

// Now running PEE Mode
  MCG_C2|=0X80;// генерируется сброс при потере внешнего clk
return pll_freq;

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,265 Views
melissa_hunter
NXP Employee
NXP Employee

Hi Nataliya,

On the Kinetis devices with a DDR controller, there is a fixed divide by 2 from the PLL VCO frequency that I think you aren't taking into account. Here's the PLL section of the MCG block diagram:

PLL.png

Notice the /2 block on the right side.

So to clock the core at 150MHz you do actually want a VDIV of 36 :

25MHz * (36/3) /2 = 150 MHz MCGCLKOUT

Hope this helps,

Melissa

View solution in original post

0 Kudos
Reply
2 Replies
1,266 Views
melissa_hunter
NXP Employee
NXP Employee

Hi Nataliya,

On the Kinetis devices with a DDR controller, there is a fixed divide by 2 from the PLL VCO frequency that I think you aren't taking into account. Here's the PLL section of the MCG block diagram:

PLL.png

Notice the /2 block on the right side.

So to clock the core at 150MHz you do actually want a VDIV of 36 :

25MHz * (36/3) /2 = 150 MHz MCGCLKOUT

Hope this helps,

Melissa

0 Kudos
Reply
1,265 Views
nataliyadoni
Contributor I

Hi Melissa,

Thank you for help. You are absolutly right.

0 Kudos
Reply