TeraTerm can not communicate with FRDM-KL25 Z

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TeraTerm can not communicate with FRDM-KL25 Z

1,494件の閲覧回数
mahmoud72
Contributor I

Hi,

I have a program written in ARM assembly language, the task is to display a character on TeraTerm terminal. I have tried to run the program using different version of Keil microvision MDK522, MDK521a and MDK513 but it did not work with any of them. my code is correct because when I have tested it with a PC at laboratory, it worked fine. I am using Teraterm version 4.93. I am using FRDM-KL25Z evaluation board and the debugger is PEMicro Debugger.

Thanks

ラベル(2)
0 件の賞賛
返信
1 返信

1,204件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Mahmoud AI-Quzwini,

   Before you testing, you must make sure you are using the correct uart port in your code.

  You can refer to our official sample code for FRDM-KL25 which can be download from this link:

Welcome to Kinetis Expert | Kinetis Expert

 Download FRDM-KL25 KSDK2.0 package. use the helloword project.

  Please use the official code, and try again.

If you still have question, please let me know!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信