TWR-k60 default Handler

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

TWR-k60 default Handler

跳至解决方案
3,400 次查看
ivanrobles
Contributor III

I'm trying to debug my code step by step about CAN. I have my main.c as:

int main(void)

{

  uint32 MBRxID = 0x659; //Mail box RX ID

  uint32 MBTxID = 0x82; //Mail box TX ID

  uint08 BytesReceived = 0; //Bytes read from CAN bus

  uint32 GetID;

  uint16 BaudRate = 1000; //1 Mbit/s

  uint32 Data0Received = 0; //Data read from MB

  uint32 Data1Received = 0; //Data read from MB

  uint32 Data0Send = 0x12345678; //Data that will be sent

  uint32 Data1Send = 0x98765432;      //Data that will be sent

  uint08 NumBytesTX = 8; //Number of bytes that will be sent

  /* Init FlexCAN module, Clock, interrupts and GPIO*/

  FlexCAN1Init();

  /* Config the FlexCAN module and Baud rate */

  FlexCAN1Config(BaudRate);

  /* Prepare Mailbox to receive */

  FlexCAN1PrepareMBRX(MBRxID, FLEXCAN_MB9, FLEXCAN_STD_DATA_FRAME, FLEXCAN_MB_asRX);

  /* Prepare Mailbox to transmit */

  FlexCAN1PrepareMBTX(MBTxID, Data0Send, Data1Send, FLEXCAN_MB8, FLEXCAN_STD_DATA_FRAME, FLEXCAN_MB_asTX,NumBytesTX);

  for(;;)

  {  

  FlexCAN1TransmitMB(FLEXCAN_MB8);

  do

  {

  BytesReceived = FlexCAN1Receive(&GetID, Data0Received, Data1Received);

  }while(!BytesReceived);

  }

  return 0;

}

When the debug enters in  FlexCAN1Init(); function, it configure the clock and the port. After, the debug sends me to the function

void Default_Handler()

{

  __asm("bkpt");

}

It inside in kinetis_sysinit.c and the code never exists of there, How do I fix it?

标签 (1)
1 解答
3,037 次查看
ivanrobles
Contributor III

Hello Monica,

Yes I have. The issue was that the Clock for the PORTE wasn't set.

thank you so much!!! :smileywink:

在原帖中查看解决方案

0 项奖励
回复
4 回复数
3,038 次查看
ivanrobles
Contributor III

Hello Monica,

Yes I have. The issue was that the Clock for the PORTE wasn't set.

thank you so much!!! :smileywink:

0 项奖励
回复
3,037 次查看
egoodii
Senior Contributor III

You might also benefit from a 'better' fault-handler, such as that I have gleaned from some Freescale projects and attached here.  If the fault is a write-access, you will get 'imprecise' information, as writes are buffered.  To force a precise capture of information (for debug, as this is a performance penalty) you can turn that off:

SCB_ACTLR |= SCB_ACTLR_DISDEFWBUF_MASK;

Note that this vector table is specific to a K20-100, and is only 'generally related' to a K60 table.

3,037 次查看
Monica
Senior Contributor III

Hello Ivan,

Have this suggestions been helpful? Please keep us posted, we'd like to know :smileywink:

Best,

Monica.

0 项奖励
回复
3,037 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Please check if during FlexCAN1Init() function, it enabled the FlexCAN1 clock gate before the FlexCAN1 module related registers access.

You could enable FlexCAN1 clock gate with below code:

SIM_SCGC3 |= SIM_SCGC3_FLEXCAN1_MASK;

Freescale also provides FlexCAN example code, please check [can_loopback_node] example with below link:

KINETIS512_SC  : Kinetis family example projects.

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=K60_100&nodeId=01624698C9DE2DDDAF&fps...

Wish it helps.

B.R.

Ma Hui

0 项奖励
回复