TWR-LCD Using FlexBus from K70

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TWR-LCD Using FlexBus from K70

1,874件の閲覧回数
awesomeclaw
Contributor I

Hello, I'm trying to get the TWR-LCD module working via FlexBus from a TWR-K70F120M. I can get the screen to display content over SPI just fine, but I can't get any output when using the FlexBus interface. I read that there are problems with the IR circuitry interfering with FlexBus (www.utasker.com/docs/.../uTaskerV1.4_Kinetis_demo.pdf - page 10) and that the solution is to either remove some components from the board or cut a trace. Is this the case? Thanks!

[EDIT] OK, I neglected to mention that I was using an MQX project. It seems that when using the same Flexbus/LCD code on a bareboard project the LCD works correctly. Presumably then there is some problem with using Flexbus with MQX. I'll open a new question/discussion for that.

タグ(5)
0 件の賞賛
返信
1 返信

1,293件の閲覧回数
ankurchauhan
Contributor I

Hi Herry:

I'm also trying to use LCD via flexbus interface on the same kit(k70) but in bareboard project.

can you share some sample code of that.

Regards

Ankur

0 件の賞賛
返信