TWR-LCD-RGB Power Supply

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TWR-LCD-RGB Power Supply

Jump to solution
2,745 Views
elisamejia
Contributor III

Hi all,

I'm developing a project using TWR-K70 development board and the TWR-LCD-RGB. I need to use the screw terminal to supply the system, because in my final product I will not have access to a USB port.

What I'm doing right now is supplying the system with a DC power supply. This needs to be high due to the other circuits I'm using, so it is around 18 to 24 volts. I'm using several stages to diminish this voltage to 5 volts using linear voltage regulators. However, these are getting really hot and suddenly the LCD is not getting enough current and turns down. I'm not sure why this is happening because apparently the system is using only 480 mA and the different regulators I'm using (LM7815, 7812, 7809 and 7805) are capable of supplying twice this current.

Is there any recommended supply system for this issue?

Regards,

Elisa

0 Kudos
Reply
1 Solution
2,533 Views
inigofs
Contributor I

Hello Elisa,

Can you show us how did you arrange those linear regulators?

BTW the best option could be using a buck converter not a linear regulator.

View solution in original post

2 Replies
2,534 Views
inigofs
Contributor I

Hello Elisa,

Can you show us how did you arrange those linear regulators?

BTW the best option could be using a buck converter not a linear regulator.

2,533 Views
elisamejia
Contributor III

Hi Inigo,

The arrange was pretty simple, just regulating the voltage in different stages from 24 to 5 volts, so each regulator didn't have such a big drop in the voltage. However, using just one buck converter it was solved.

Thanks for your help,

Elisa

0 Kudos
Reply