TWR-KV58F220M

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TWR-KV58F220M

Jump to solution
1,692 Views
a8Chcx
Contributor IV

Hi,

I am testing demo application for now. And have the following questions:

1) KV58F220M can work on 240Mhz as well? If not, what is the maximum frequency on this?

2) In the demo project, it is set to 235.7Mhz, is it any reason why not set to 240MHz?

Thanks,

Christie

Labels (1)
0 Kudos
Reply
1 Solution
1,529 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Christie,

Pls go to the website:

ARM Cortex-M7|Kinetis KV5x Real-time Control MCUs|NXP 

all of KV5x can work in 240mhz at most in high speed run mode.

Because the TWR-KV58 uses external 50MHz external clock source, and the PLL input clock frequency must range from 8mhz to 16MHz, so this is the PLL configuration

VCO output clock frequency=(50MHz/4)*19*2=475MHz, PLL output clock frequency is 475MHz/2=237.5MHz.

The external 50mhz clock source is populated on the TWR-KV58 board and it is the clcok souce for Ethernet.

Hope it can help you

BR

XiangJun Rong

View solution in original post

0 Kudos
Reply
1 Reply
1,530 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Christie,

Pls go to the website:

ARM Cortex-M7|Kinetis KV5x Real-time Control MCUs|NXP 

all of KV5x can work in 240mhz at most in high speed run mode.

Because the TWR-KV58 uses external 50MHz external clock source, and the PLL input clock frequency must range from 8mhz to 16MHz, so this is the PLL configuration

VCO output clock frequency=(50MHz/4)*19*2=475MHz, PLL output clock frequency is 475MHz/2=237.5MHz.

The external 50mhz clock source is populated on the TWR-KV58 board and it is the clcok souce for Ethernet.

Hope it can help you

BR

XiangJun Rong

0 Kudos
Reply