TWR-KM35Z75M U2 VOUT

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TWR-KM35Z75M U2 VOUT

1,513件の閲覧回数
cheekun
Contributor I

Hello.

Regarding U2 of TWR-KM35Z75M, pin 2 is connected to the 3.3V power line in the schematic, but pin 3 is connected to the 3.3V power line in the Gerber and the actual board. This is probably the reason why a voltage of about 3.9V is supplied to the MCU, which exceeds the required operating conditions. How can I make this board supply a voltage to the MCU within the required operating conditions?

Best regards

0 件の賞賛
返信
3 返答(返信)

1,491件の閲覧回数
Celeste_Liu
NXP Employee
NXP Employee

Hello @cheekun ,

Thanks for your post.

Do you mean there is a discrepancy between our reference board and the schematic diagram? Or is it your custom board that has this issue?
Is the setting of your Jumper J3 correct?
Please refer to the TWR-KM35Z75M-QSG. 

Celeste_Liu_0-1744601666758.pngCeleste_Liu_0-1744601666758.png

The doc can be downloaded from TWR-KM35Z75M | Tower System Board | KM MCUs | NXP | NXP Semiconductors

Celeste_Liu_1-1744602248808.pngCeleste_Liu_1-1744602248808.png

Hope it can help you.

BRs,

Celeste

0 件の賞賛
返信

1,468件の閲覧回数
cheekun
Contributor I

Celeste

Thank you for your quick response.

Yes. I think there is the difference between the reference board schematic and artwork design. The jumper on J3 is connected. However, it is possible that the board does not output 3.3V correctly regardless of the jumper on J3.

 

0 件の賞賛
返信

1,368件の閲覧回数
Celeste_Liu
NXP Employee
NXP Employee

Hello @cheekun ,

Sorry for the late reply. My TWR-KM35Z75M was borrowed. I just got it back and conducted the test. 

In fact, I have already measured and obtained the following values:

J3-3.316 V
J6-3.316 V

U2
Pin3 - 3.3165 V
Pin2 - 4.895 V

It doesn't seem to have the problems as you described. Could you please double-check it again? Thanks for your understanding.

Have a nice day.

Celeste

 

0 件の賞賛
返信