TWR-K70F120M

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TWR-K70F120M

1,922 Views
jeemonjoy
Contributor II

Hello,

In current KSDK version 1.0.0, support for TWR-K70F120M seems to be not there. In order to start working with the board, from where shall I find its supporting demo projects and library files?.

Thanks in advance

Regards,..

Jeemon Joy

2 Replies

1,783 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Jeemon:

You can start by downloading the sample code package called "KINETIS_120MHZ_SC" under "Snippets, Boot Code, Headers, Monitors, etc" from the next link:

K70_120 |Kinetis K70 120/150 MHz MCUs|Freescale

The examples are available for IAR and CodeWarrior.


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,783 Views
jeemonjoy
Contributor II

Hi Gonzalez,

Thanks for your reply.

I am not using IAR and CodeWarrior but Kinetis Design Studio. Do TWR-K70F120M have any support in Kinetis Design Studio with out using Processor  Expert?.

Regards,

Jeemon Joy

0 Kudos
Reply