TWR-K60N512 reset problem prevents reprogramming

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

TWR-K60N512 reset problem prevents reprogramming

1,167 次查看
flav1
Contributor I

Hi!

I'm working with the TWR-K60N512 board and I wanted to configure the FLL. But now, when I'm resetting the microcontroller, the reset pin stay to the low level (I measured it), and it's impossible to reprogram it with the OSJTAG. I think it's because of an anormal comportment of the microcontroller which prevent its communication with the embedded OSBDM. The only way to have the microcontroller working is to disconnect and reconnect the board.

I want to know if there is a way to erase all the internal flash thanks to the OSJTAG or the jumper configuration to remove this comportment and to let me reprogram the component.

Best regards,

Flavien

标签 (1)
标记 (4)
0 项奖励
回复
2 回复数

1,076 次查看
mjbcswitzerland
Specialist V

Hi Flavien

Try with CodeWarrior with the Hardware Connection properties set to perform an erase on connection:

pastedImage_0.png

This can be used to erase when SW behavior is otherwise immediately causing the debugger difficuties.

Regards

Mark

Kinetis: http://www.utasker.com/kinetis.html

K60: µTasker Kinetis TWR-K60N512 support / µTasker Kinetis TWR-K60D100M support / µTasker Kinetis TWR-K60F120M support

For the complete "out-of-the-box" Kinetis experience and faster time to market

0 项奖励
回复

1,076 次查看
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello flav1:

There are ways to perform a mass erase. The procedure depends however in your IDE or available tools.

Please provide more details about what software you are using (e.g. CodeWarrior, IAR, Keil).

Regards!

Jorge Gonzalez

0 项奖励
回复