TWR-K60N512 - USB HID MOUSE DEVICE - MQX

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

TWR-K60N512 - USB HID MOUSE DEVICE - MQX

跳至解决方案
3,308 次查看
andreidamiandas
Contributor II

Hi, I'm having a problem running the usb hid mouse device demo, using mqx 3.8.1, using TWR-K60N512. I tried with mqx 3.7 too and got the same error: "Device could not be initialized". I tried with the default jumper configuration, also with J6 in pins 1-2, and clock in serial to 50, as is showed in the manual, same error.

Now it is set like in those pictures, except that I have jumpers in all J5 pins:

https://community.freescale.com/servlet/JiveServlet/download/301654-251093/2012-09-26_20-43-13_768.j...

https://community.freescale.com/servlet/JiveServlet/download/301654-251103/2012-09-26_20-42-51_459.j...

I tried with windows XP and 7, different usb ports, reinstalled driver, changed elevator sockets, nothing changes.

Do you believe that could be a jumper configuration or the board is damaged?

Also, what is the purpose of jumper J4 in serial module?

标签 (2)
标记 (5)
0 项奖励
回复
1 解答
2,760 次查看
andreidamiandas
Contributor II

Fixed... it was a jumper configuration, I will submit pictures later.

在原帖中查看解决方案

0 项奖励
回复
4 回复数
2,760 次查看
soledad
NXP Employee
NXP Employee

Hi, 

Do you have this issue only with the usb hid mouse device demo?

Do you have this issue if you run a hello world??

0 项奖励
回复
2,760 次查看
andreidamiandas
Contributor II

Only with usb hid mouse device demo... hello world is ok, adc example works too.

0 项奖励
回复
2,761 次查看
andreidamiandas
Contributor II

Fixed... it was a jumper configuration, I will submit pictures later.

0 项奖励
回复
2,760 次查看
Monica
Senior Contributor III

Great you were able to fix it up Andrei! And thanks for sharing the solution, we'll be waiting for the pictures.

Best regards!

0 项奖励
回复