TWR-K60N512 MCU datasheet

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TWR-K60N512 MCU datasheet

1,567件の閲覧回数
pasini
Contributor I

Can anyone show me how I can find the full datasheet for the MCU from the tower TWR-K60N512 ? I just cannot find the information regarding pinout, registers peripheral configuration. Where do I find these things ?

I guess ( not sure !!! ) the MCU is MK60DN512VMD10 . The only datasheet I found is for K60P144M100SF2V2 . Are they the same ?

What about registers, peripheral configuration ? Where can I find this information ?

Freescale datasheet system is really confusing....

Thanks in advance,

Luiz

タグ(3)
0 件の賞賛
返信
2 返答(返信)

1,435件の閲覧回数
mjbcswitzerland
Specialist V

Luiz

For the TWR-K60N512:

http://cache.freescale.com/files/32bit/doc/ref_manual/TWR-K60N512-UM.pdf?fpsp=1

For the circuit diagrams you need to use the "Download" tab:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=TWR-K60N512-IAR&fpsp=1&tab=Design_Too... (Printed Circuit Boards and Schematics)

The TWR-K60N512 is an old board and has an old Kinetis part on it (not recommended for new products and possible no longer manufactured).

Its data sheets and user manuals are at:

http://cache.freescale.com/files/microcontrollers/doc/data_sheet/K60P144M100SF2.pdf?fasp=1&WT_TYPE=D...

http://cache.freescale.com/files/microcontrollers/doc/data_sheet/K60P144M100SF2.pdf?fasp=1&WT_TYPE=D...

Regards

Mark

Kinetis: µTasker Kinetis support

K60: µTasker Kinetis TWR-K60N512 support / µTasker Kinetis TWR-K60D100M support / µTasker Kinetis TWR-K60F120M support

For the complete "out-of-the-box" Kinetis experience and faster time to market

0 件の賞賛
返信

1,435件の閲覧回数
ivadorazinova
NXP Employee
NXP Employee

Hello Luiz Melek,

Yes. MK60DN512VMD10.

please, here is datasheet http://cache.freescale.com/files/32bit/doc/data_sheet/K60P144M100SF2V2.pdf

Probably you mean Reference Manual, please go http://cache.freescale.com/files/32bit/doc/ref_manual/K60P144M100SF2V2RM.pdf

Everything is located on our websites.

If you go to K60_100 |Kinetis K60 100 MHz MCUs|Freescale on the left side Reference Manual and other Documentation.

I hope it helps,

Iva

0 件の賞賛
返信