TWR-K60N512-IAR code example.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

TWR-K60N512-IAR code example.

跳至解决方案
4,684 次查看
Mendes
Contributor I

How do we get the code example of TWR-K60N512 IAR without having to buy the kit?

0 项奖励
回复
1 解答
3,704 次查看
mnorman
NXP Employee
NXP Employee

Mendes,

 

The TWR-K60N512 Quick Start Demo (QSD) source code and lab guide are available on the TWR-K60N512 tool support page here:

http://www.freescale.com/twr-k60n512

 

Here is a direct link to the zip file: TWRK60N512QSDLAB 

 

The QSD  demo application is an MQX application.  You can get the latest MQX BSP, including support for the Kinetis family, from the web here: http://www.freescale.com/mqx

 

-mnorman

在原帖中查看解决方案

0 项奖励
回复
3 回复数
3,705 次查看
mnorman
NXP Employee
NXP Employee

Mendes,

 

The TWR-K60N512 Quick Start Demo (QSD) source code and lab guide are available on the TWR-K60N512 tool support page here:

http://www.freescale.com/twr-k60n512

 

Here is a direct link to the zip file: TWRK60N512QSDLAB 

 

The QSD  demo application is an MQX application.  You can get the latest MQX BSP, including support for the Kinetis family, from the web here: http://www.freescale.com/mqx

 

-mnorman

0 项奖励
回复
3,704 次查看
Bill256
Contributor I

How do I get a copy of the original binary file that was shipped in my new TWR-K60N512 Tower unit?

 

The Terminal Demo (as explained in the Quick Start Demo) worked fine when I took my Tower out of the box, but now that I have worked through the rest of the Lab, the Terminal Demo no longer works. The Touch Demo, the Accelerometer Demo, the Memory Game, and the Web Server Demo work fine, but the Terminal Demo does NOT work anymore. I would like to have the original binary file (and instructions on how to load it) so that I can see if I broke something doing the Lab (or not).

 

Thanks,

 

Bill

0 项奖励
回复
3,704 次查看
anthony_huereca
NXP Employee
NXP Employee

If everything else works, the most likely problem is a driver issue with OSJTAG. Look at Section 8 of the lab guide for troubleshooting tips. Make sure the PEMicro USB Serial Port is actually being enumerated.

0 项奖励
回复