TWR-K60N512-IAR code example.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TWR-K60N512-IAR code example.

Jump to solution
4,550 Views
Mendes
Contributor I

How do we get the code example of TWR-K60N512 IAR without having to buy the kit?

0 Kudos
Reply
1 Solution
3,570 Views
mnorman
NXP Employee
NXP Employee

Mendes,

 

The TWR-K60N512 Quick Start Demo (QSD) source code and lab guide are available on the TWR-K60N512 tool support page here:

http://www.freescale.com/twr-k60n512

 

Here is a direct link to the zip file: TWRK60N512QSDLAB 

 

The QSD  demo application is an MQX application.  You can get the latest MQX BSP, including support for the Kinetis family, from the web here: http://www.freescale.com/mqx

 

-mnorman

View solution in original post

0 Kudos
Reply
3 Replies
3,571 Views
mnorman
NXP Employee
NXP Employee

Mendes,

 

The TWR-K60N512 Quick Start Demo (QSD) source code and lab guide are available on the TWR-K60N512 tool support page here:

http://www.freescale.com/twr-k60n512

 

Here is a direct link to the zip file: TWRK60N512QSDLAB 

 

The QSD  demo application is an MQX application.  You can get the latest MQX BSP, including support for the Kinetis family, from the web here: http://www.freescale.com/mqx

 

-mnorman

0 Kudos
Reply
3,570 Views
Bill256
Contributor I

How do I get a copy of the original binary file that was shipped in my new TWR-K60N512 Tower unit?

 

The Terminal Demo (as explained in the Quick Start Demo) worked fine when I took my Tower out of the box, but now that I have worked through the rest of the Lab, the Terminal Demo no longer works. The Touch Demo, the Accelerometer Demo, the Memory Game, and the Web Server Demo work fine, but the Terminal Demo does NOT work anymore. I would like to have the original binary file (and instructions on how to load it) so that I can see if I broke something doing the Lab (or not).

 

Thanks,

 

Bill

0 Kudos
Reply
3,570 Views
anthony_huereca
NXP Employee
NXP Employee

If everything else works, the most likely problem is a driver issue with OSJTAG. Look at Section 8 of the lab guide for troubleshooting tips. Make sure the PEMicro USB Serial Port is actually being enumerated.

0 Kudos
Reply