TWR-K60F120M

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TWR-K60F120M

1,471 Views
jgreene
Contributor I

Hello,

I could use some help getting an SD card up and running on TWR-K60F120M. I've been having a difficult time locating resources on the proper way to initialize this "module". I have enabled a memory card via the "Run-Time Environment" feature in Keil. The issue I'm now having is that finit("M0:") hangs but fmount("M0:") does not. Could someone please let me know the appropriate way of initializing the file system?

Below is an empty project I'm using to test with:

 

 

#include <stdio.h>
#include "rl_fs.h"
#include "cmsis_os2.h"
#include "system_MK60F12.h"

volatile int test = 0;

int main (void)  {
   SystemInit();
   //osKernelInitialize ();
   volatile fsStatus test2 = finit ("M0:");
   //volatile fsStatus test3 = fmount ("M0:");
   //volatile fsStatus test2 = finit ("");
   
   while(1)
   {
      if(test++ > 500)
      {
         test = 0;
      }
      
   }
   
   return 0;
}

void Driver_SPI0(void)
{
}

 

 

 

0 Kudos
Reply
1 Reply

1,447 Views
mjbcswitzerland
Specialist V

Hi

I don't have any experience with the Keil SD card interface but if you license it from them you could ask them directly.

Otherwise there is professionally supported, off-the-shelf solution that also works with Keil at https://www.utasker.com/kinetis/TWR-K60F120M.html which allows you to immediately use the SD card by the application, including for USB-MSD or FTP/Web server usage.

It is also available in open source form if no support is required at https://github.com/uTasker/uTasker-Kinetis (also with Keil project) and allows you to simulate the TWR board, the K60F and SD card in Visual Studio.

Regards

Mark
[uTasker project developer for Kinetis and i.MX RT]
Contact me by personal message or on the uTasker web site to discuss professional training, solutions to problems or product development requirements

 

0 Kudos
Reply