TWR-K60D100M USB problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TWR-K60D100M USB problem

1,284 Views
MWMinor
Contributor V

Hi

Can anyone help me with a problem I have trying to get the USB port on the TWR-SER board to work as a CDC device...?

I've checked links on the TWR-SER board and they are correct;

pastedImage_0.png

and tried using both the virtual com port and the mouse example but neither work.....and by working I mean that when I plug the mini-usb connector to a spare USB port on my laptop, the laptop just doesn't see it.

I've tried another laptop - but that made no difference.

I know the port on the TWR-SER card works, as when I tried the HVAC demo, the boards respond when the USB stick is plugged in it enumerates and mounts the disk.

If anyone has any suggestions they would be really appreciated.

Ken

0 Kudos
Reply
1 Reply

1,070 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Ken:

We are sorry you did not receive help with this issue before. I see you just posted a new thread in the following link:

Problem with USB enumeration on K60 board

I will follow up with you with that new one.

Regards!
Jorge Gonzalez

0 Kudos
Reply