TWR-K60D100M Developer's board,

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TWR-K60D100M Developer's board,

2,009 Views
imrankhan
Contributor II

Hi Forum,

I have TWR-K60D100 developer board with MCU with USB and Ethernet port with an Encryption such as DES1 DES3 AES SHA1 SHA256 and RSA with in communicating over the SPI Bus to FPGA, it is a low powered device. I am hoping to figure out following

1/ Currently there were no documentation or supporting software CD/DVD etc as far too many engineer worked and given up, hence therefore, I have to get developer tools and source code to get started?

2/ I cannot find any thing free of on an Internet as a dev tools. I was hoping to get Linux Developer tool chain over Fed 20 with ARM Compiler and tool chain for TWR-K60 board

3/ But scavenging whole net past few weeks yielded nothing as this Board Does not have MMU hence therefore limited use of boot loader LINUX kernel is out of the question.

4/ Currently TWR-K60 does not communicate over JTAG using a minicom or any serial communication.

5/ My target is to get the source code for TWR K60 which I understood to be a bare metal version of ARM

6/ Build the source code image and upload in to board to bring up

7/ It seems to be communication issue over USB or serial port while my Fedora 20 running as on VM Box

8/ Board seems to be lightening up but no communication with Host hence no possibility to upload OS

9/ Do have to use Window based Code warrior dev tool from freescale?

0/ If any one can shed a light on this subject please, as I only have Fedora 20 with GNU Tool chain with ARM Compiler and its tool chain.

I will be grateful if you any one can put me in the right direction please.

Thank you,

IK

0 Kudos
Reply
2 Replies

1,842 Views
yarannan
Contributor III

For No.4, I would suggest you go to PEmicro website and try to update firmware. Thats how I fixed mine but on Windows platform.

0 Kudos
Reply

1,842 Views
mjbcswitzerland
Specialist V

Hi

Check µTasker Kinetis TWR-K60D100M support to verify that your board is OK.

You can use CodeWarrior and the board's integrated debugger (free for code sizes up to 128k) or KDS. Another completely free tool chain is CooCox.

If you want to use uCLinux you can move to a K61 or K70 and use EmCraft's distribution: Freescale Kinetis K70 System-On-Module (SOM)

Regards

Mark

Kinetis: µTasker Kinetis support

K60: µTasker Kinetis TWR-K60N512 support / µTasker Kinetis TWR-K60D100M support / µTasker Kinetis TWR-K60F120M support

For the complete "out-of-the-box" Kinetis experience and faster time to market

0 Kudos
Reply