TWR-K60 Communications code examples

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TWR-K60 Communications code examples

ソリューションへジャンプ
4,411件の閲覧回数
apanecatl
Senior Contributor II

I received a question from one of our customers asking for code examples to use in the TWR-K60, if you check the code example folders:

Right under snippets, boot code, etc...

https://community.freescale.com/community/kinetis/post!input.jspa?containerType=14&container=2019

You can find examples for CAN, USB, EThernet, SPI, I2C and UART protocols

Thanks to ivanrobles for pointing my attention to the fact that we do not specify which code examples are included in which files, I hope this answers your question.

ラベル(1)
1 解決策
2,367件の閲覧回数
apanecatl
Senior Contributor II

You are correct, the 120MHz code examples are not there, here is the correct link

KINETIS_120MHZ_SC

Right under snippets, boot code, etc...

https://community.freescale.com/community/kinetis/post!input.jspa?containerType=14&container=2019


元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,367件の閲覧回数
ivanrobles
Contributor III

Ok I understand that these examples are for Kinetis 60 100 MHz, but I need examples for Kinetis K60 120 MHz and I don´t find examples about CAN for TWR-K60F120M only I find them for TWR-K60N152. They are similar debuggers. I took the example SC12CAN from TWR-K60N152 and I adapted for TWR-K60F120M but I don´t know if this example code works in my TWR-K60F120M for this reason I need to test but I don´t know how

I followed the instructions for test this example code with the terminal, I´m trying to test SCI2CAN demo and RXfifo demo, but when I choose SCI2CAN demo, it order me that put any character in the terminal and the CAN will respond me and I will see that character but  I don´t see it. When I choose RXfifo demo I can see the data, I don´t have problem whit this demo.

2,368件の閲覧回数
apanecatl
Senior Contributor II

You are correct, the 120MHz code examples are not there, here is the correct link

KINETIS_120MHZ_SC

Right under snippets, boot code, etc...

https://community.freescale.com/community/kinetis/post!input.jspa?containerType=14&container=2019


0 件の賞賛
返信