TSI in LLWU Settings

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,492件の閲覧回数
javervalino
Contributor III

Hello All,

We have another problem arise in our hardware setup. We found out that when you use TSI0_CH0 in external pin 1 in   LLWU settings, you cannot use it as electrode pin in TSS_library component.

Please see below image.

15058_15058.pngTSI0_ CH0.png

Can it be solved by using the internal module 4 (TSI0) instead? Can somone give an example how to use TSI as internal module. Our product requires to wake-up from LLS mode using TSI in PEx.

15057_15057.pngInternal module 4 (TSI0).png

Thank you and best regards,

Javer

ラベル(1)
タグ(4)
0 件の賞賛
返信
1 解決策
2,318件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Javer,

I just answered your question in your another thread, please kindly refer to Re: Re: Exiting Low Power Modes Using TSI in Processor Expert for details.

Hope that helps,


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,318件の閲覧回数
javervalino
Contributor III

Hello All,

Any suggestion?

Thanks,

Javer

0 件の賞賛
返信
2,319件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Javer,

I just answered your question in your another thread, please kindly refer to Re: Re: Exiting Low Power Modes Using TSI in Processor Expert for details.

Hope that helps,


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信