TSI Versions

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TSI Versions

2,082件の閲覧回数
Frotz
Contributor III

Hi,

I'm working on a project requiring a touch interface. I'm looking at the KL25/26/28 and the KE15/16 MCU's. I see that the KL's use TSI v4 and the KE's use TSI v5. But I can't find a summary of the differences between the different TSI versions. Does anyone know the advantages/disadvantages of the two? So far I can find that v5 works with self AND mutual cap, where as v4 seems to be self only. Are there more differences? Perhaps there's a PDF somewhere that explains the enhancements. 

Thank you very much,

Andre.

ラベル(2)
タグ(1)
0 件の賞賛
返信
1 返信

2,076件の閲覧回数
nxf56274
NXP Employee
NXP Employee

Hi,

Here is the document for you to refer. TSI

1.PNG

 

4.PNG

 

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信