TPMS Receiver

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TPMS Receiver

2,744 Views
amitkhan
Contributor I

Since MRB-KW019032NA is no longer manufactured, I was thinking of using FRDM-KW019032. Do you think this is a good substitute?

I am trying to develop a receiver for FXTH870xD (TPMS Sensor) and require a dev board, ideally controlled from hyperterminal/serial/usb and with RF ports. Do you know of any dev board?

Is there an easy way to change MRB-KW019032JA to MRB-KW019032NA? I noticed that the XTAL is different.

Any suggestions would be greatly appreciated.

Note: I am trying to replicate https://www.nxp.com/docs/en/application-note/AN5136.pdf 

Tags (3)
0 Kudos
Reply
3 Replies

2,420 Views
amitkhan
Contributor I

Hi,

The FRDM-KW019032 board only comes in China variant. Is there a NA variant that is available for purchase?

What is the main difference between the CHN and NA variants? Is it just the XTAL?

Thank You,

0 Kudos
Reply

2,420 Views
stephanie_m
NXP TechSupport
NXP TechSupport

Have you checked the Distributor Network|NXP  ? 

Regards, 

Estephania

0 Kudos
Reply

2,420 Views
stephanie_m
NXP TechSupport
NXP TechSupport

Hello, 

Actually, the best fit for what you are looking for with one of our current solutions for SubGHz it's the FRDMKW01 and you will need to migrate the project available FXTH87|Tire Pressure Monitor Sensor|NXP  to fit the MCU in the FRDM. 

About the board of the TPMS sensor, I was able to locate two different information sources that might be helpful for you:

https://www.nxp.com/docs/en/reference-manual/FXTH87EDRM.pdf 

https://community.nxp.com/thread/336038 

Regards, 

Estephania

0 Kudos
Reply