T=1oI2C

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 
3,865 Views
nidhintomy
Contributor IV

What is the meaning of T = 1 in T1oI2C ?

 

0 Kudos
Reply
1 Solution
3,788 Views
danielchen
NXP TechSupport
NXP TechSupport

Yes, you are right.

T=0:  asynchronous half duplex character transmission

T=1: asynchronous half duplex block transmission.

 

 

View solution in original post

4 Replies
3,859 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi @nidhintomy :

 

T =1 is a peer to peer, half duplex transmission protocol defined in ISO/IEC 7816-3.  T=1 protocol usage is very common in the smart card domain.

Please refer to UM11225 for more details.

https://www.nxp.com/webapp/sps/download/preDownload.jsp?render=true

 

Regards

Daniel

3,855 Views
nidhintomy
Contributor IV

Hi @danielchen

Is ' T ' means ' Transmission ' and ' 1 ' means the ' 1 ' block of data mentioned in UM11225 ?

Thanks

0 Kudos
Reply
3,789 Views
danielchen
NXP TechSupport
NXP TechSupport

Yes, you are right.

T=0:  asynchronous half duplex character transmission

T=1: asynchronous half duplex block transmission.

 

 

3,776 Views
nidhintomy
Contributor IV

@danielchen 

Thanks for clarification.

0 Kudos
Reply