System Integration Module of MKE1xZ

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

System Integration Module of MKE1xZ

1,905 次查看
nehayadav
Contributor I

Hi,

I am working on NXP MKE1xZ256 board. I am currently writing code to run an application that requires to read core Id, flash size and ram size of mcu. I searched it's reference manual and find out that SIM(System Integration Module) peripheral can provide me this information.

My Query is:

"How to exactly get core id, flash size and ram size of mcu from SIM peripheral ?"

Please Support !NXP Community—New Features, New Functionality, New Platform mke14 mke15 mke15z256vlh7 ke15z kinetis ke1xz #cortexm0#cortex m0#cortex-m0+#cotex m0+#cortex-m0#mke15z##nxp‌ 

0 项奖励
回复
1 回复

1,857 次查看
sabinesjaime82
Contributor I

I don't know which IDE or SDK you are using however writting a simple code:

You can directly read the SIM_FCFG1 register using a 32 bit variable to know  Program flash size

Read SIM_SDID register using another variable to know RAM size.

And read Unique Identification Registers as the following post suggest

How to read the unique ID for K60? 

Also, take a look at the reference manual, and perform the necesary masks to get the correct values.

You can use MCUXpresso IDE and install a Ke1xz SDK to do a mini project with this porpuse. 

0 项奖励
回复