Support for I2S peripherals on MCUXpresso Pin Tool?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Support for I2S peripherals on MCUXpresso Pin Tool?

ソリューションへジャンプ
1,937件の閲覧回数
2bluesc
Contributor II

Hi,

I was playing the the MCUXpresso Pin Tool and noticed that the I2S peripheral isn't available for the KL27.  Are there plans to add more peripherals to the tool?  It would be a great help and seems to be the only thing missing from this tool.

Thanks!

ラベル(2)
タグ(3)
1 解決策
1,769件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Kyle Manna,

Please check the part number of your MCU. The part number listed below should support I2S.

MKL27Z128VFM4
MKL27Z128VFT4
MKL27Z128VLH4
MKL27Z128VMP4
MKL27Z256VFM4
MKL27Z256VFT4
MKL27Z256VLH4
MKL27Z256VMP4

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
---------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
1,770件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Kyle Manna,

Please check the part number of your MCU. The part number listed below should support I2S.

MKL27Z128VFM4
MKL27Z128VFT4
MKL27Z128VLH4
MKL27Z128VMP4
MKL27Z256VFM4
MKL27Z256VFT4
MKL27Z256VLH4
MKL27Z256VMP4

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
---------------------------------------------------------------------------------------------------------------------

1,769件の閲覧回数
2bluesc
Contributor II

Ahh yes, I made the mistake of starting with the FRDM-KL27 which was a KL27Z64.


All better, thanks for the help!

0 件の賞賛
返信