Support for I2S peripherals on MCUXpresso Pin Tool?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Support for I2S peripherals on MCUXpresso Pin Tool?

Jump to solution
1,963 Views
2bluesc
Contributor II

Hi,

I was playing the the MCUXpresso Pin Tool and noticed that the I2S peripheral isn't available for the KL27.  Are there plans to add more peripherals to the tool?  It would be a great help and seems to be the only thing missing from this tool.

Thanks!

1 Solution
1,795 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Kyle Manna,

Please check the part number of your MCU. The part number listed below should support I2S.

MKL27Z128VFM4
MKL27Z128VFT4
MKL27Z128VLH4
MKL27Z128VMP4
MKL27Z256VFM4
MKL27Z256VFT4
MKL27Z256VLH4
MKL27Z256VMP4

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
---------------------------------------------------------------------------------------------------------------------

View solution in original post

2 Replies
1,796 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Kyle Manna,

Please check the part number of your MCU. The part number listed below should support I2S.

MKL27Z128VFM4
MKL27Z128VFT4
MKL27Z128VLH4
MKL27Z128VMP4
MKL27Z256VFM4
MKL27Z256VFT4
MKL27Z256VLH4
MKL27Z256VMP4

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
---------------------------------------------------------------------------------------------------------------------

1,795 Views
2bluesc
Contributor II

Ahh yes, I made the mistake of starting with the FRDM-KL27 which was a KL27Z64.


All better, thanks for the help!

0 Kudos
Reply