Storage for AES Keys

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Storage for AES Keys

1,808 Views
dspNeil
Contributor III

AN4235 mentions secure storage of encryption keys in the MPC564 via the CSE (Crytpographic Services Engine). Does the Kinetis have any such write-only storage that could be used to securely store AES encryption keys for use with the CAU (Cryptographic Acceleration Unit)?

 

It seems counterintuitive to encrypt when the keys can simply be read from flash...

0 Kudos
Reply
1 Reply

1,454 Views
BenGartner
Contributor II

Setting certain bitfields at 0x0_040C will prevent the chip's flash from being read by debug devices Look for the Flash Security register FSEC. This data is also mirror in the register FTFL_FSEC. This will effect the entire flash of the chip, but this is good practice if there are security concerns.

0 Kudos
Reply