Source code for CM4_MMCLIB and CM4_ACLIB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Source code for CM4_MMCLIB and CM4_ACLIB

1,149 Views
ilantiagai
Contributor I

Hi, is the source code for CM4_MMCLIB library (the library containing motor control, general math, and filter algorithms) and  the CM4_ACLIB library (advanced control algorithms for rotor position) available anywhere?

0 Kudos
Reply
1 Reply

1,061 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Ilan,

You can download the embedded Software Motor Control and Power Conversion Libraries from this page:

Embedded Software Motor Control and Power Con|NXP

Hope it helps!

Best Regards,

Carlos Mendoza

Technical Support Engineer

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply