Source code for CM4_MMCLIB and CM4_ACLIB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Source code for CM4_MMCLIB and CM4_ACLIB

1,172件の閲覧回数
ilantiagai
Contributor I

Hi, is the source code for CM4_MMCLIB library (the library containing motor control, general math, and filter algorithms) and  the CM4_ACLIB library (advanced control algorithms for rotor position) available anywhere?

0 件の賞賛
返信
1 返信

1,084件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Ilan,

You can download the embedded Software Motor Control and Power Conversion Libraries from this page:

Embedded Software Motor Control and Power Con|NXP

Hope it helps!

Best Regards,

Carlos Mendoza

Technical Support Engineer

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信