Source Code for K60 Serial Bootloader?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Source Code for K60 Serial Bootloader?

Jump to solution
3,790 Views
danielchai
Senior Contributor I

Hi All,

Where could I find the source code for the serial bootloader for K60?

Thank you.

-Daniel

0 Kudos
Reply
1 Solution
3,160 Views
anthony_huereca
NXP Employee
NXP Employee

Hi Daniel,

  You can find the software package here, which has K60 projects: Software for AN2295

  Also in order to save pins, by default the bootloader does not use a pin to enter bootloader mode, it uses the UART. This is configurable though. See section 2.1 of the app note.

Regards,

Anthony

View solution in original post

0 Kudos
Reply
4 Replies
3,160 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

please search an2295 in Freescale web site, it covers serial bootloader for kinetis.

3,160 Views
danielchai
Senior Contributor I

Hi Jun,

I read the AN2295, but there is no code for K60. One more thing is that if I want K60 to go to bootloader, which pin should I pull low?

Thank you.

3,161 Views
anthony_huereca
NXP Employee
NXP Employee

Hi Daniel,

  You can find the software package here, which has K60 projects: Software for AN2295

  Also in order to save pins, by default the bootloader does not use a pin to enter bootloader mode, it uses the UART. This is configurable though. See section 2.1 of the app note.

Regards,

Anthony

0 Kudos
Reply
3,160 Views
dominikf
Contributor II

The link was down. With some searching I found the source code package here: http://cache.freescale.com/files/microcontrollers/doc/app_note/AN2295SW.zip

Cheers,

Dominik

0 Kudos
Reply