Software UART (using the FTM or TPM)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Software UART (using the FTM or TPM)

Software UART (using the FTM or TPM)

The attached zip file contains software that accompanies the document UART Emulation Using the FTM or TPM.  It contains two sample applications:  one that uses the TPM, and one that uses the FTM. The TPM example targets the FRDM-KL26Z development board and is written in baremetal code.  The FTM example targets the TWR-K22F120M and FRDM-K22F and is written using the Kinetis SDK 1.0 release. 

Installation instructions are contained within the zip package. Unzip the package to an empty folder and then copy the appropriate folders to the the appropriate locations on your PC per the instructions located in the zip file. 

附件
无评分
版本历史
最后更新:
‎01-26-2015 01:42 PM
更新人: