Simple (non-sdk) deep sleep example - wake from PB - FRDM-K22F

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Simple (non-sdk) deep sleep example - wake from PB - FRDM-K22F

1,667 Views
mjg8t
Contributor IV

I have struggled with the complexity of the power_manager example to put the K22F to deep sleep.  The example is much too complex to easily simplify to use a bare bones non-sdk project. 

Wondering if an NXP rep or someone else can help by providing a simple go to deep sleep project which wakes from a pushbutton for the FRDM-K22F board.  This would help me greatly in getting a time crunched project out the door.  

Thanks for any help provided.  

0 Kudos
Reply
2 Replies

1,437 Views
isaacavila
NXP Employee
NXP Employee

Hello,

Here you can find a basic document and example (in baremetal) that sets MCU to lowest power modes (LLS and VLLSx):

Power Management on Kinetis MCUs: LLS and VLLS modes 

It is focused on KL26 device but same principle will apply to FRDM-K22F.

I hope you can find it useful!

Regards,

Isaac Avila

0 Kudos
Reply

1,437 Views
mjbcswitzerland
Specialist V

Hi Michael

See: http://www.utasker.com/kinetis/LLWU.html

Then see http://www.utasker.com/kinetis/FRDM-K22F.html which allows you to choose any LLWU mode and wake up from it using a push button (either temporarily to do one operation or permenently to RUN mode, or from a RTC alarm).


If you need an immediate and complete solution just take the uTasker project (it is bare-metal in the sense of your requirements) and includes complete power management support integrated with no more work (as well as almost everything else that the K22 could need, plus a K22 simulator that allows the complete project to be tested in (approx.) real-time, excercising peripherals, interrupt, DMA etc...).

Regards


Mark
Kinetis for professionals: http://www.utasker.com/kinetis.html

0 Kudos
Reply