Silicon versions for MK10 processor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Silicon versions for MK10 processor

1,277 Views
danlowe
Contributor I

I need to purchase some MK10DX256VLQ10 processors but none are available atm.

The MK10DX256ZVLQ10 is available but it is using "initial" silicon instead of "main" silicon.

Does anyone know what the difference is between these two versions of silicon and whether the MK10DX256ZVLQ10 is a suitable replacement for the MK10DX256VLQ10?

Any help would be much appreciated.

Thanks

0 Kudos
Reply
1 Reply

1,273 Views
nxf56274
NXP Employee
NXP Employee

Hi,

The 'initial' means that it is the 1.x silicon. 'main' means that it is the 2.x silicon. You can refer this document. If possible, please do not use the old silicon.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply