Silicon versions for MK10 processor

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Silicon versions for MK10 processor

1,273件の閲覧回数
danlowe
Contributor I

I need to purchase some MK10DX256VLQ10 processors but none are available atm.

The MK10DX256ZVLQ10 is available but it is using "initial" silicon instead of "main" silicon.

Does anyone know what the difference is between these two versions of silicon and whether the MK10DX256ZVLQ10 is a suitable replacement for the MK10DX256VLQ10?

Any help would be much appreciated.

Thanks

0 件の賞賛
返信
1 返信

1,269件の閲覧回数
nxf56274
NXP Employee
NXP Employee

Hi,

The 'initial' means that it is the 1.x silicon. 'main' means that it is the 2.x silicon. You can refer this document. If possible, please do not use the old silicon.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信