Serial wire debug pin is pulled down/up internally.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Serial wire debug pin is pulled down/up internally.

ソリューションへジャンプ
2,169件の閲覧回数
jun1
Contributor V

Please kindly advise.

I have a question about SWD hardware.

In the manual "Document Number: MKMxxZxxACxx5RM Rev. 1, 09/2014"
"9.2 Debug Port Pin Descriptions" has the following description.

Serial Wire Clock. This pin is the clock for debug logic when in Serial Wire Debug mode. This pin is pulled down internally.
Serial wire debug data input / output. The SWD_IO pin is used by an external debug tool for communication and device control.

There are SWD_CLK pull-down and SWD_IO pull-up.
I have a question about this.
① What is the value of this pull-up resistor and pull-down resistor?
② Does it not have to pull up pulled down externally?
    Or should I do it?
③ If the pull-up / pull-down is required, how much resistance?

I do not have good English.

Thank you.

ラベル(1)
1 解決策
2,028件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

① internal 30 kΩ to 60 kΩ
② It does not have to pull up pulled down externally. But external pull resistors are recommended.
③ external 4.7 kΩ to 10 kΩ

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
2,029件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

① internal 30 kΩ to 60 kΩ
② It does not have to pull up pulled down externally. But external pull resistors are recommended.
③ external 4.7 kΩ to 10 kΩ

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------