Serial wire debug pin is pulled down/up internally.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Serial wire debug pin is pulled down/up internally.

跳至解决方案
2,205 次查看
jun1
Contributor V

Please kindly advise.

I have a question about SWD hardware.

In the manual "Document Number: MKMxxZxxACxx5RM Rev. 1, 09/2014"
"9.2 Debug Port Pin Descriptions" has the following description.

Serial Wire Clock. This pin is the clock for debug logic when in Serial Wire Debug mode. This pin is pulled down internally.
Serial wire debug data input / output. The SWD_IO pin is used by an external debug tool for communication and device control.

There are SWD_CLK pull-down and SWD_IO pull-up.
I have a question about this.
① What is the value of this pull-up resistor and pull-down resistor?
② Does it not have to pull up pulled down externally?
    Or should I do it?
③ If the pull-up / pull-down is required, how much resistance?

I do not have good English.

Thank you.

标签 (1)
1 解答
2,064 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

① internal 30 kΩ to 60 kΩ
② It does not have to pull up pulled down externally. But external pull resistors are recommended.
③ external 4.7 kΩ to 10 kΩ

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

1 回复
2,065 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

① internal 30 kΩ to 60 kΩ
② It does not have to pull up pulled down externally. But external pull resistors are recommended.
③ external 4.7 kΩ to 10 kΩ

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------