Selecting Internal Flash Memory to flash OTAP_ATT Freertos/bm code - Using IAR

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Selecting Internal Flash Memory to flash OTAP_ATT Freertos/bm code - Using IAR

ソリューションへジャンプ
16,700件の閲覧回数
Vishva
Contributor II

Hi,

I have followed the below procedure to configure OTAP Client software in IAR Workbench

https://community.nxp.com/t5/Wireless-Connectivity-Knowledge/KW38-Reprogramming-a-KW38-device-using-...

When i modify the otap_client_att source code to use Internal Flash memory as given in the above link, I'm getting following errors,

Error[Li005]: no definition for "INT_STORAGE_START"

Error[Li005]: no definition for "INT_STORAGE_SECTOR_SIZE"

Error[Li005]: no definition for "INT_STORAGE_SIZE"

Note : Configuring External memory works fine.

Kindly check and let me know how to resolve this issue.

Thanks in advance

 

0 件の賞賛
返信
1 解決策
16,567件の閲覧回数
EdgarLomeli
NXP Employee
NXP Employee

Hi @Vishva,

I found that in the post there is a typo. I did a mistake writing the name of the linker flag that needs to be set to 1 for internal storage.

The proper name is "gUseInternalStorageLink_d=1". See the picture below:

EdgarLomeli_0-1649344058606.pngEdgarLomeli_0-1649344058606.png

Could you please try to build the OTAP Client again with this linker flag?

Best regards.

Edgar. 

 

 

元の投稿で解決策を見る

7 返答(返信)
16,568件の閲覧回数
EdgarLomeli
NXP Employee
NXP Employee

Hi @Vishva,

I found that in the post there is a typo. I did a mistake writing the name of the linker flag that needs to be set to 1 for internal storage.

The proper name is "gUseInternalStorageLink_d=1". See the picture below:

EdgarLomeli_0-1649344058606.pngEdgarLomeli_0-1649344058606.png

Could you please try to build the OTAP Client again with this linker flag?

Best regards.

Edgar. 

 

 

16,654件の閲覧回数
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @Vishva,

Seems the predefine for the storage has been update, please change the previous one for this:

gUseInternalStorageLink_d = 1;

BR,

Alexis Andalon

16,632件の閲覧回数
Vishva
Contributor II

Hi Alexis,

@Alexis_A 

I tried changing the settings as you suggested. Refer to the LinkerSettings.png

Following change is done in app_preinclude.h
#define gEepromType_d gEepromDevice_InternalFlash_c

--------------------------------------
Still i got the following errors,

Error[Li005]: no definition for "INT_STORAGE_START" [referenced from D:\xxxx\boards\frdmkw38\wireless_examples\bluetooth\w_uart\freertos\iar\debug\obj\framework\OtaSupport\OtaSupport.o]

Error[Li005]: no definition for "INT_STORAGE_SECTOR_SIZE" [referenced from D:\xxxx\boards\frdmkw38\wireless_examples\bluetooth\w_uart\freertos\iar\debug\obj\framework\Flash\External\source\Eeprom_InternalFlash.o]

Error[Li005]: no definition for "INT_STORAGE_SIZE" [referenced from D:\xxxx\boards\frdmkw38\wireless_examples\bluetooth\w_uart\freertos\iar\debug\obj\framework\OtaSupport\OtaSupport.o]

---------------------------------------
I have tried to move the variables to OtaSupport.c file which resolved the issues(COMPILATION SUCCESSFUL) but follwoing warnings are there,

Warning[Pe1682]: array variable "INT_STORAGE_SIZE" assumed to have one element D:\xxxx\middleware\wireless\framework\Flash\External\interface\Eeprom.h 88
Warning[Pe1682]: array variable "INT_STORAGE_START" assumed to have one element D:\xxxx\middleware\wireless\framework\Flash\External\interface\Eeprom.h 89
Warning[Pe1682]: array variable "INT_STORAGE_SECTOR_SIZE" assumed to have one element D:\xxxx\middleware\wireless\framework\Flash\External\interface\Eeprom.h 90
Warning[Pe1682]: array variable "Image$$INT_STORAGE$$Base" assumed to have one element D:\xxxx\boards\frdmkw38\wireless_examples\bluetooth\w_uart\freertos\iar\debug\BrowseInfo\framework\OtaSupport\source\OtaSupport.c 29
Warning[Pe1682]: array variable "Image$$INT_STORAGE$$Length" assumed to have one element D:\xxxx\boards\frdmkw38\wireless_examples\bluetooth\w_uart\freertos\iar\debug\BrowseInfo\framework\OtaSupport\source\OtaSupport.c 30

-------------------------------------------
But after flashing the code, unable to do OTA update. Firmware update hangs in 0-1%.
Refer to FirmwareUpdateScreen.png


Please check and let me know.

Thanks in advance.

0 件の賞賛
返信
16,618件の閲覧回数
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @Vishva,

Can you tell me which SDK version are you using?

BR,
Alexis Andalon

0 件の賞賛
返信
16,616件の閲覧回数
Vishva
Contributor II

Hi @Alexis_A ,

SDK version "SDK_2_6_12_FRDM-KW38"

Thanks,

Vishva

0 件の賞賛
返信
16,609件の閲覧回数
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @Vishva,

The latest SDK right now is the 2.6.14, could you try updating to the latest one?

BR,

Alexis Andalon

0 件の賞賛
返信
16,674件の閲覧回数
Vishva
Contributor II

In Continuation with the previous query,

As we know OTA Image file can be stored in FlexNVM (Internal) or External flash available on FRDMKW38.

But why to write OTA image file, internal storage (P-flash) from 0x3e800 - 0x3d000 is selected in the example given?

Please refer to the attachment.

Please check and let me know how to use Internal flash (FlexNVM) to store OTA Image files.

Thanks

0 件の賞賛
返信