Segger - Error while launching command: arm-none-eabi-gdb --version

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Segger - Error while launching command: arm-none-eabi-gdb --version

跳至解决方案
16,671 次查看
amuresan
Contributor III

I get this error when I'm using Segger

pastedImage_1.png

I selected the segger configuration

arm-none-eabi-gdb  

Why doesn't this work?

0 项奖励
回复
1 解答
16,029 次查看
amuresan
Contributor III

I figured it out:

I had to manually specify the highlighted field

pastedImage_1.png

在原帖中查看解决方案

0 项奖励
回复
12 回复数
16,030 次查看
amuresan
Contributor III

I figured it out:

I had to manually specify the highlighted field

pastedImage_1.png

0 项奖励
回复
16,030 次查看
BlackNight
NXP Employee
NXP Employee

Can you share/show your launch configuration settings?

That message usually tells you that it was not able to find binary, see Troubleshooting Tips: Failed Debugging with GDB | MCU on Eclipse 

I hope this helps,

Erich

0 项奖励
回复
16,031 次查看
amuresan
Contributor III

No it doesn't help.

KDS is calling the wrong executable: it's not supposed to be calling "arm-none-eabi-gdb" for the SEGGER.

pastedImage_1.png

I set the Segger GDB path

pastedImage_2.png

0 项奖励
回复
16,031 次查看
BlackNight
NXP Employee
NXP Employee

you have the launch config wrong:

pastedImage_1.png

You need to specify a project there.

And yes: gdb is the client talking to the SEGGER gdb server, see Command Line Programming and Debugging with GDB | MCU on Eclipse 

I hope this helps,

Erich

0 项奖励
回复
16,031 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Adrain Muresan,

   What's the chip part number you are using now? Do you use the official board or your own designed board?

   At first, I suggest you use the JLINK commander to check whether you can find the ARM core or not?

   If even JLINK commander which in the JLINK driver install path also can't find the ARM core, it means your hardware have problems, you need to check the hardware connections.

  Please test this point at first, and give me the the JLINK commander screen shoot.

With is helps you!

Have a great day,
Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复
16,031 次查看
amuresan
Contributor III

pastedImage_2.png

0 项奖励
回复
16,031 次查看
BlackNight
NXP Employee
NXP Employee

If you already have the GDB server running locally (see Command Line Programming and Debugging with GDB | MCU on Eclipse ), then you shall not launch yet another copy, so uncheck this:

pastedImage_190.png

I hope this helps,

Erich

0 项奖励
回复
16,031 次查看
amuresan
Contributor III

I did. Still same issue.

pastedImage_1.png

0 项奖励
回复
16,031 次查看
BlackNight
NXP Employee
NXP Employee

Do not start the J-Link Server exectuable externally. Let the debugger launch it (unless you know exactly what you are doing).

And do not forget to specify the project name (see other reply).

I hope this helps,

Erich

0 项奖励
回复
16,031 次查看
amuresan
Contributor III

I tried switching to MCUXpresso but alas, you guys appear to not want to support SEGGER.

https://community.nxp.com/message/1118972 

0 项奖励
回复
16,032 次查看
amuresan
Contributor III

If I don't start it externally and I uncheck that box, how is the server launched?

Also I'm pretty sure I started it correctly.

pastedImage_1.png

0 项奖励
回复
16,032 次查看
BlackNight
NXP Employee
NXP Employee

It starts the server locally (as indicated in the checkbox).

0 项奖励
回复