Sample code I2S for MK20DX128VLH5 repost

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Sample code I2S for MK20DX128VLH5 repost

2,846 Views
afdasdfas
Contributor II

Hi all. Does any one have sample code or project  I2S for Kinetis MK20DX128VLH5 Or code of any any kinetis MCU ? I try to find it so much, but don't see any thing to refer . I need to build I2S for audio use MK20DX128VLH5.  But There are too little information or tutorial or support or project about Kinetis.

Tags (1)
0 Kudos
Reply
4 Replies

2,102 Views
carlos_neri
NXP Employee
NXP Employee

take a look to this thread, it has an example that might be useful:

https://community.freescale.com/message/81904#81904

0 Kudos
Reply

2,102 Views
LuisCasado
NXP Employee
NXP Employee

Hello,

Have you seen these AN?

http://cache.freescale.com/files/32bit/doc/app_note/AN4369.pdf?fpsp=1&WT_TYPE=Application Notes&WT_VENDOR=FREESCALE&WT_FILE_FORMAT=pdf&WT_ASSET=Documentation

http://cache.freescale.com/files/32bit/doc/app_note/AN4800.pdf?fpsp=1&WT_TYPE=Application Notes&WT_VENDOR=FREESCALE&WT_FILE_FORMAT=pdf&WT_ASSET=Documentation

Luis

2,102 Views
afdasdfas
Contributor II

Hi

Thank you. These AN are helpful for me to know I2S, but i donot know the way to build the actual I2S project on CodeWarrior . Do you have any project about i2s which i can refer to build my project ?

Huynh Viet Phuong

0 Kudos
Reply

2,102 Views
LuisCasado
NXP Employee
NXP Employee

Hello,

Do you mean that you can't build the software projects associated to the application notes?

Luis

0 Kudos
Reply