SWD protocol test on read/write register

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SWD protocol test on read/write register

SWD protocol test on read/write register

The board used: FRDM-KE02

SWD: The ARM Serial Wire Debug interface uses a single bidirectional data connection(SWDIO) and a separate clock (SWDCLK) to transfer data synchronously. An operation on the wire consists of two or three phases:

Packet request       The external host debugger issues a request to the DP. The DP is the target of the request.

Acknowledge response   The target sends an acknowledge response to the host.

Data transfer phase

First enter into SWD mode: Send at least 50 SWCLKTCK cycles with SWDIOTMS HIGH and 0xE79E. This ensures that the current interface is in its reset state and enable the SWD mode.

uint8_t SWJ_JTAG2SWD(void)
{
    uint32_t i;
    SWDIO_SET();
    for(i = 0; i < 56; i++)
    {
        SW_CLOCK_CYCLE();
    }
    SWJ_SendData(0xE79E);//SWJ_SendData(0xB76D);以后遇到再加
    for(i = 0; i < 56; i++)
    {
        SW_CLOCK_CYCLE();
    }
    SWDIO_CLR();
    for(i = 0; i < 16; i++)
    {
        SW_CLOCK_CYCLE();
    }
    return 0;

}

Then write DP/AP register. A successful write operation is as below:

pastedImage_7.png

DP Register:
Address     Read              Write
0x00        IDCODE           ABORT
0x04        CTRL/STAT      CTRL/STAT
0x08        RESEND           SELECT
0x0C        RDBUFF           N/A

Address     Read              Write
0x00         CSW               CSW
0x04         TAR               TAR
0x08         N/A                N/A
0x0C         DRW              DRW
0xFC         IDR                N/A

Read IDCODE:
uint8_t SWJ_ReadDP(uint8_t adr, uint32_t *val)
{
    uint32_t tmp_in;
    uint8_t ack;
    uint8_t err;


    tmp_in = SWD_REG_DP | SWD_REG_R | SWD_REG_ADR(adr);
    ack = SWD_Transfer(tmp_in, val);


    (ack == DAP_TRANSFER_OK) ? (err = 0) : (err = 1);
    return err;
}

uint8_t SWJ_ReadAP(uint32_t adr, uint32_t *val)
{
    uint8_t tmp_in, ack, err;


    uint32_t apsel = adr & APSEL;
    uint32_t bank_sel = adr & APBANKSEL;


    if(SWJ_WriteDP(DP_SELECT, apsel | bank_sel))
    {
        return 1;
    }

tmp_in = SWD_REG_AP | SWD_REG_R | SWD_REG_ADR(adr);


    /* first dummy read */
    ack = SWD_Transfer(tmp_in, val);
    ack = SWD_Transfer(tmp_in, val);


    (ack == DAP_TRANSFER_OK) ? (err = 0) : (err = 1);
    return err;
}

評価なし
バージョン履歴
最終更新日:
‎03-28-2018 08:47 AM
更新者: