SWD general purpose serial communication

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SWD general purpose serial communication

ソリューションへジャンプ
1,963件の閲覧回数
gschelotto
Contributor V

Hi,

I'd like to develop a firmware running on any FRDM-Kxx that is capable of RAM writing/reading on/from a KE02 device through SWD debug port by SWO and SWI pins. Is it feasible? How?

regards,

gaston

0 件の賞賛
返信
1 解決策
1,737件の閲覧回数
mjbcswitzerland
Specialist V

Gaston

You can take the OpenSDA project (it is available as source I believe) which generally runs on a K20 (or similar) and supposedly bit-bangs the SWD protocol to read/write/program/debug SWD based processors.

You should be able the use the same routines to do what you want to do.

Alternatively you can take any FRDM-Kx board and use its on-board OpenSDA interface connected to other boards - there are various tutorials/blogs about doing this - eg. https://mcuoneclipse.com/2014/08/09/hacking-the-teensy-v3-1-for-swd-debugging/

Regards

Mark

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,737件の閲覧回数
mjbcswitzerland
Specialist V

Gaston

You can take the OpenSDA project (it is available as source I believe) which generally runs on a K20 (or similar) and supposedly bit-bangs the SWD protocol to read/write/program/debug SWD based processors.

You should be able the use the same routines to do what you want to do.

Alternatively you can take any FRDM-Kx board and use its on-board OpenSDA interface connected to other boards - there are various tutorials/blogs about doing this - eg. https://mcuoneclipse.com/2014/08/09/hacking-the-teensy-v3-1-for-swd-debugging/

Regards

Mark

0 件の賞賛
返信